|
EPD Extension Kit for MSP430 LaunchPad
|
The SPI, PWM, Temperature definitions of COG hardware driver. More...
#include "Pervasive_Displays_small_EPD.h"Go to the source code of this file.
Macros | |
| #define | SMCLK_FREQ (16000000) |
| #define | __External_Temperature_Sensor |
| #define | SPISEL P1SEL |
| #define | SPISEL2 P1SEL2 |
| #define | SPIIE IE2 |
| #define | SPICTL0 UCB0CTL0 |
| #define | SPICTL1 UCB0CTL1 |
| #define | SPIBR0 UCB0BR0 |
| #define | SPIBR1 UCB0BR1 |
| #define | SPIMCTL UCA0MCTL |
| #define | SPIIFG IFG2 |
| #define | SPIRXBUF UCB0RXBUF |
| #define | SPIRXIFG UCB0RXIFG |
| #define | SPITXBUF UCB0TXBUF |
| #define | SPITXIFG UCB0TXIFG |
| #define | SPISTAT UCB0STAT |
| #define | SPI_baudrate (SMCLK_FREQ/COG_SPI_baudrate) |
Functions | |
| void | spi_init (void) |
| Configure SPI. | |
| void | spi_attach (void) |
| Initialize SPI. | |
| void | spi_detach (void) |
| Disable SPI and change to GPIO. | |
| void | SPI_send (unsigned char Register, unsigned char *Data, unsigned Length) |
| SPI command if register data is larger than two bytes. More... | |
| void | SPI_send_byte (uint8_t Register, uint8_t Data) |
| SPI command. More... | |
| uint8_t | SPI_read (unsigned char RDATA) |
| SPI synchronous read. | |
| void | SPI_write (unsigned char Data) |
| SPI synchronous write. | |
| uint8_t | SPI_write_ex (unsigned char Data) |
| Send data to SPI with time out feature. More... | |
| void | sys_delay_ms (unsigned int ms) |
| Delay mini-seconds. More... | |
| void | start_EPD_timer (void) |
| Start Timer. | |
| void | stop_EPD_timer (void) |
| Stop Timer. | |
| uint32_t | get_current_time_tick (void) |
| Get current Timer after starting a new one. | |
| void | PWM_start_toggle (void) |
| The PWM signal starts toggling. | |
| void | PWM_stop_toggle (void) |
| The PWM signal stops toggling. | |
| void | PWM_run (uint16_t time) |
| PWM toggling. More... | |
| void | initialize_temperature (void) |
| Initialize the temperature sensor. | |
| int16_t | get_temperature (void) |
| Get temperature value from ADC. More... | |
| void | EPD_display_hardware_init (void) |
| Initialize the EPD hardware setting. | |
The SPI, PWM, Temperature definitions of COG hardware driver.
Copyright (c) 2012-2013 Pervasive Displays Inc. All rights reserved.
Authors: Pervasive Displays Inc.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
| #define SPI_baudrate (SMCLK_FREQ/COG_SPI_baudrate) |
the baud rate of SPI
| #define SPISEL P1SEL |
SPI Defines
| int16_t get_temperature | ( | void | ) |
Get temperature value from ADC.
| void PWM_run | ( | uint16_t | ms | ) |
PWM toggling.
| ms | The interval of PWM toggling (mini seconds) |
| void SPI_send | ( | unsigned char | register_index, |
| unsigned char * | register_data, | ||
| unsigned | length | ||
| ) |
SPI command if register data is larger than two bytes.
| register_index | The Register Index as SPI command to COG |
| register_data | The Register Data for sending command data to COG |
| length | The number of bytes of Register Data which depends on which Register Index is selected. |
| void SPI_send_byte | ( | uint8_t | register_index, |
| uint8_t | register_data | ||
| ) |
SPI command.
| register_index | The Register Index as SPI command to COG |
| register_data | The Register Data for sending command data to COG |
| uint8_t SPI_write_ex | ( | unsigned char | Data | ) |
Send data to SPI with time out feature.
| data | The data to be sent out |
| void sys_delay_ms | ( | unsigned int | ms | ) |
Delay mini-seconds.
| ms | The number of mini-seconds |
1.8.3.1